AXIS#.SAFE.FSOE.WATCHDOGTIME

Description

The current FSoE watchdog time in milliseconds. If an FSoE packet is not received within the configured time the drive enters a safe state. This is configured by using the FSoE master.

Context

For complete FSoE information refer to the AKD2G EtherCAT Manual.

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read Only

Units

N/A

Range

7 to 65535

Default Value

100

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFE.FSOE.WATCHDOGTIME

e901h

04h

Unsigned16

-

-

Read only

No

AXIS2.SAFE.FSOE.WATCHDOGTIME

e911h

04h

Unsigned16

-

-

Read only

No